BSP setup for LPDDR memory?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BSP setup for LPDDR memory?

ソリューションへジャンプ
2,699件の閲覧回数
jrasmussen
Contributor II

I'm trying to put in the parameters for the LPDDR memory we are using in the DDR controller registers, and was really surprised to see that we need 64 registers worth of values.  I wanted to check if someone has already used and/or setup this memory in the BSP for the K70?  The routine for initializing the DDR2 memory is in the init_hw.c file of the MQX BSP.  Do we need to initialize values in all of the registers, or can we skip some portions of these DDR registers?

We are using the Micron MT46H8M16LF-6 memory part.

Thanks,

--James

0 件の賞賛
返信
1 解決策
2,385件の閲覧回数
jrasmussen
Contributor II

Thanks.  I was able to get an init routine from Freescalse exports that I used to replace to DDR2 initialization sequence in the BSP with our LPDDR initialization.  All is working well now.

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,385件の閲覧回数
gnelly
Contributor I

We are also looking for the LPDDR init routine for our MQX BSP.

Where can we get more information for obtaining this code?

Thank you.

Gary

0 件の賞賛
返信
2,385件の閲覧回数
johannesschock
Contributor II

Hello.

We're also looking for a LPDDR-init routine.

Can you James or anybody else publish it?

Thanks in advance.

Johannes

0 件の賞賛
返信
2,385件の閲覧回数
LANCO_M4
Contributor II

Check with your local Freescale FAE. Freescale has a DDR utility that helps setup the registers based on the DDR chip you are using. We used it for DDR-I on our board.

0 件の賞賛
返信
2,386件の閲覧回数
jrasmussen
Contributor II

Thanks.  I was able to get an init routine from Freescalse exports that I used to replace to DDR2 initialization sequence in the BSP with our LPDDR initialization.  All is working well now.

 

 

0 件の賞賛
返信