BSP for MK22FN1M0VMC12

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BSP for MK22FN1M0VMC12

3,673 Views
sudhanshumehta
Contributor IV

Hi All,

I have "MK22FN1M0VMC12" controller on my board.

Do we have MQX BSP for this controller? I do not find it in MQX4.2 examples or KSDK 1.3.

if we have, can you please provide me some link. If not, do we have some basic BSP on which I can do changes,

another thing can we have some demo board for having "MK22FN1M0VMC12".

I an not looking for any other part number.

Thanks

Sudhanshu..

0 Kudos
Reply
4 Replies

3,354 Views
soledad
NXP Employee
NXP Employee

Hello Sudhanshu,

MQX 4.2 and MQX for KSDK have support for the FRDM-K22F (MK22FN512VLH12 MCU) and the TWR-K22F120M (K22FN512VDC12 MCU) . You can use any of  these BSP's in order to clone your own BSP.

However, these boards are supported only for KDS, Keil or IAR unfortunately there is no support for CodeWarrior.

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,354 Views
sudhanshumehta
Contributor IV

HI Soledad,

Thanks for your response..

Do you have some instructions for cloning BSP.

Thanks

Sudhanshu

0 Kudos
Reply

3,352 Views
soledad
NXP Employee
NXP Employee

Hello Sudhanshu,

Sorry for my delay. Please check the below thread and the attached documents:

Creating MQX 4.0 BSP for K10


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,352 Views
sudhanshumehta
Contributor IV

It will be good if i get BSP for Codewarrior

0 Kudos
Reply