BOOT Sequence in MQX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,629件の閲覧回数
K_Family
Contributor I

Hi friends,

 

I am working with Kinetis K60 microcontroller (TOWER K60N512 Kit + IAR + MQX 3.6),  and we are in the analysis stage of the project, hence can anyone tell me about the boot sequence of MQX in general, because i am not able to find any document regarding the MQX boot sequence.

 

0 件の賞賛
返信
1 解決策
1,299件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi K-Family,

The best way to learn the boot sequence is really to run a simple program and when debugging, set the debugger to start at the beginning of the code base and then step on through.  We don;t have documentation to that level that I know of. Sorry.

Good example to start with:

FSLMQX/mqx/examples/hello project.

In general the very low level code initializes the processor, then initializes the RTOS and whatever BSP drivers were enabled, and then looks to find the first task to start running and run it.

Hope this helps.

Regards,

David

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,300件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi K-Family,

The best way to learn the boot sequence is really to run a simple program and when debugging, set the debugger to start at the beginning of the code base and then step on through.  We don;t have documentation to that level that I know of. Sorry.

Good example to start with:

FSLMQX/mqx/examples/hello project.

In general the very low level code initializes the processor, then initializes the RTOS and whatever BSP drivers were enabled, and then looks to find the first task to start running and run it.

Hope this helps.

Regards,

David

0 件の賞賛
返信