Adding RTCS to a Processor Expert Project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Adding RTCS to a Processor Expert Project

1,952件の閲覧回数
ramstell
Contributor III

I have created a Project using KSDK/Processor Expert and have successfully added MQX (Standard), but now I wish to add RTCS.

This functionality does not seem to be supported by Processor Expert, so after reading other threads I've attempted to do this manually without complete success.

Can some one please confirm the following requirements:

Preprocessor defines

Preprocessor Include paths.

Library include paths.

Libraries

PEX hardware initialisation

PEX peripheral/HAL

Is the ability to add RTCS using Processor Expert going to be available in the future?

I'm using KDS 3.0.0, KSDK 1.2 and MQX 4.2 with a TWR-K64F120M board.

Kind regards

Roger

0 件の賞賛
返信
2 返答(返信)

1,677件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Roger,

Here you go How to add RTCS to a Processor Expert Project Using KDS and KSDK

I would appreciate your comments.

Regards,

Carlos

0 件の賞賛
返信

1,677件の閲覧回数
ramstell
Contributor III

Hi Carlos

Thank you for that, followed the instructions and all works great so far.

Kind regards

Roger

0 件の賞賛
返信