Adding RAM under MQX 4.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Adding RAM under MQX 4.1

ソリューションへジャンプ
2,614件の閲覧回数
oscargarciaabad
Contributor III

Hi all,

I'm using a custom board based on the tower TWR-K60F120M running MQX 4.1.

I'm running out of ram, so I'm very keen to add more RAM to the system.

Can anybody tell me if there is an application note on that issue? If not, how Can I implement this, and which is the type of RAM I should use?

Best regards,

Óscar.

1 解決策
2,348件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Oscar,

Attached you can find a simple example in CW10.5 and MQX4.1 (will work in CW10.6 also). Please note that you must enable in user_config.h the macros mentioned in AN4393 and rebuild MQX libraries.

Regards,

Carlos

元の投稿で解決策を見る

4 返答(返信)
2,349件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Oscar,

Attached you can find a simple example in CW10.5 and MQX4.1 (will work in CW10.6 also). Please note that you must enable in user_config.h the macros mentioned in AN4393 and rebuild MQX libraries.

Regards,

Carlos

2,348件の閲覧回数
oscargarciaabad
Contributor III

Hi Carlos,

Many thanks for your help!

Best regards.

Óscar.

0 件の賞賛
返信
2,348件の閲覧回数
Luis_Garabo
NXP TechSupport
NXP TechSupport

Hi Oscar,

I beleive you will find this appnote interesting:

AN4393


Regards,
Garabo

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,348件の閲覧回数
oscargarciaabad
Contributor III

Hi Garabo,

This is very interesting.

Many thanks for your help.

Best regards,

Óscar

0 件の賞賛
返信