ADC only works running from MRAM MCF52259EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC only works running from MRAM MCF52259EVB

Jump to solution
1,684 Views
k_dev
Contributor I

Hello All,

 

I am having some issues with the MQX ADC drivers when running from flash. The devices all open but the ADC channels never sample. When I build my code and run from MRAM everything works. I am working with the MCF52259 EVB.

 

I was curious and went to the ADC example, compiled it and programmed to flash. Running the code from flash had the same result. When running ADC example code from flash on the 52259 EVB the ADC channels will never sample, it seems that I can only get the example (and my code) to run successfully from MRAM. Any help is greatly appreciated!

 

Thanks & Best Regards,

 

Kellen

0 Kudos
Reply
1 Solution
1,067 Views
JuroV
NXP Employee
NXP Employee

It works here. Tested on MQX 3.6.1, m52259evb, Int flash Debug target.

Have you rebuilt your BSP and PSP?

 

View solution in original post

0 Kudos
Reply
2 Replies
1,068 Views
JuroV
NXP Employee
NXP Employee

It works here. Tested on MQX 3.6.1, m52259evb, Int flash Debug target.

Have you rebuilt your BSP and PSP?

 

0 Kudos
Reply
1,067 Views
k_dev
Contributor I

It seems the issue is only with MQX 3.5. I upgraded to 3.6 and have no issues.

 

Thanks!

0 Kudos
Reply