Hello Ken,
Please check the init_gpio.c file, this file is located at the path: C:\Freescale\Freescale_MQX_4_2\mqx\source\bsp\twrk60d100m
In this file you can find the function performs BSP-specific initialization related to ADC channel.
For example:
/*FUNCTION*-------------------------------------------------------------------
*
* Function Name : _bsp_adc_io_init
* Returned Value : 0 for success, -1 for failure
* Comments :
* This function performs BSP-specific initialization related to ADC
*
*END*----------------------------------------------------------------------*/
_mqx_int _bsp_adc_io_init
(
/* [IN] number of ADC device on which to perform hardware initialization */
_mqx_uint adc_num
)
{
SIM_MemMapPtr sim_ptr = SIM_BASE_PTR;
/* Enable ADC clocks */
if (adc_num == 0)
sim_ptr->SCGC6 |= SIM_SCGC6_ADC0_MASK;
else if (adc_num == 1)
sim_ptr->SCGC3 |= SIM_SCGC3_ADC1_MASK;
else
return IO_ERROR;
return IO_OK;
}
/*FUNCTION*-------------------------------------------------------------------
*
* Function Name : _bsp_adc_channel_io_init
* Returned Value : 0 for success, -1 for failure
* Comments :
* This function performs BSP-specific initialization related to ADC channel
*
*END*----------------------------------------------------------------------*/
_mqx_int _bsp_adc_channel_io_init
(
/* [IN] number of channel on which to perform hardware initialization */
uint16_t source
)
{
uint8_t ch = ADC_GET_CHANNEL(source);
uint8_t gpio_port;
PORT_MemMapPtr pctl = NULL;
#define ADC_SIG_PORTA (0x01 << 5)
#define ADC_SIG_PORTB (0x02 << 5)
#define ADC_SIG_PORTC (0x03 << 5)
#define ADC_SIG_PORTD (0x04 << 5)
#define ADC_SIG_PORTE (0x05 << 5)
#define ADC_SIG_NA (0x00) /* signal not available */
#define ADC_SIG_NC (0x01) /* signal not configurable */
/* Conversion table for ADC0x inputs, where x is 0 to 23, mux is defaultly "B" */
const static uint8_t adc0_conv_table[] = {
ADC_SIG_NC, /* 0 leave as default */
ADC_SIG_NC, /* 1 leave as default */
ADC_SIG_NC, /* 2 leave as default */
ADC_SIG_NC, /* 3 leave as default */
ADC_SIG_PORTC | 2, /* 4b */
ADC_SIG_PORTD | 1, /* 5b */
ADC_SIG_PORTD | 5, /* 6b */
ADC_SIG_PORTD | 6, /* 7b */
ADC_SIG_PORTB | 0, /* 8 */
ADC_SIG_PORTB | 1, /* 9 */
ADC_SIG_PORTA | 7, /* 10 */
ADC_SIG_PORTA | 8, /* 11 */
ADC_SIG_PORTB | 2, /* 12 */
ADC_SIG_PORTB | 3, /* 13 */
ADC_SIG_PORTC | 0, /* 14 */
ADC_SIG_PORTC | 1, /* 15 */
ADC_SIG_NC, /* 16 conflict in K60 Sub-Family Reference Manual, Rev. 5, table 3.7.1.3.1 and 10.3.1 */
ADC_SIG_PORTE | 24, /* 17 */
ADC_SIG_PORTE | 25, /* 18 */
ADC_SIG_NC, /* 19 ADC0_DM0, leave as default */
ADC_SIG_NC, /* 20 ADC0_DM1, leave as default */
ADC_SIG_NC, /* 21 conflict in K60 Sub-Family Reference Manual, Rev. 5, table 3.7.1.3.1 and 10.3.1 */
ADC_SIG_NC, /* 22 conflict in K60 Sub-Family Reference Manual, Rev. 5, table 3.7.1.3.1 and 10.3.1 */
ADC_SIG_NC, /* 23 DAC0, leave as default */
ADC_SIG_NA, /* 24 not implemented */
ADC_SIG_NA, /* 25 not implemented */
/* below: use ADC_SIG_NC (leave as default) */
};
/* Conversion table for ADC1x, where x is 0 to 23, mux is defaultly "B" (or nothing) */
const static uint8_t adc1_conv_tableB[] = {
ADC_SIG_NC, /* 0 leave as default */
ADC_SIG_NC, /* 1 leave as default */
ADC_SIG_NC, /* 2 leave as default */
ADC_SIG_NC, /* 3 leave as default */
ADC_SIG_PORTC | 8, /* 4b */
ADC_SIG_PORTC | 9, /* 5b */
ADC_SIG_PORTC | 10, /* 6b */
ADC_SIG_PORTC | 11, /* 7b */
ADC_SIG_PORTB | 0, /* 8 */
ADC_SIG_PORTB | 1, /* 9 */
ADC_SIG_PORTB | 4, /* 10 */
ADC_SIG_PORTB | 5, /* 11 */
ADC_SIG_PORTB | 6, /* 12 */
ADC_SIG_PORTB | 7, /* 13 */
ADC_SIG_PORTB | 10, /* 14 */
ADC_SIG_PORTB | 11, /* 15 */
ADC_SIG_NC, /* 16 */
ADC_SIG_PORTA | 17, /* 17 */
ADC_SIG_NC, /* 18 VREF, leave as default */
ADC_SIG_NC, /* 19 ADC1_DM0, leave as default */
ADC_SIG_NC, /* 20 ADC1_DM1, leave as default */
ADC_SIG_NA, /* 21 not implemented */
ADC_SIG_NA, /* 22 not implemented */
ADC_SIG_NC, /* 23 DAC1, leave as default */
ADC_SIG_NA, /* 24 not implemented */
ADC_SIG_NA, /* 25 not implemented */
/* below: use ADC_SIG_NC (leave as default) */
};
/* Conversion table for ADC1x, where x is 4 to 7, mux is "A" */
const static uint8_t adc1_conv_tableA[] = {
ADC_SIG_PORTE | 0, /* 4a */
ADC_SIG_PORTE | 1, /* 5a */
ADC_SIG_PORTE | 2, /* 6a */
ADC_SIG_PORTE | 3, /* 7a */
};
if (ADC_GET_DIFF(source) && ch > 3)
return IO_ERROR; /* signal not available */
if (ADC_GET_DIFF(source) == 0 && ch == 2)
return IO_ERROR; /* channel 2 (PGA) can be used only as a diff pair */
if (ch < 26) {
if (ADC_GET_MODULE(source) == ADC_SOURCE_MODULE(1)) {
/* Get result for module 0 */
gpio_port = adc0_conv_table[ch];
}
else {
if ((ADC_GET_MUXSEL(source) == ADC_SOURCE_MUXSEL_B) || (ADC_GET_MUXSEL(source) == ADC_SOURCE_MUXSEL_X))
/* Get result for module 1, if user wants "B" channel or any channel */
gpio_port = adc1_conv_tableB[ch];
else {
/* Get result for module 1, if user wants "A" channel or any other */
if (ch < 4 || ch > 7)
gpio_port = ADC_SIG_NA;
else
gpio_port = adc1_conv_tableA[ch - 4];
}
}
}
else
gpio_port = ADC_SIG_NC;
if (gpio_port == ADC_SIG_NA)
return IO_ERROR; /* signal not available */
if (gpio_port == ADC_SIG_NC)
return IO_OK; /* no need to configure signal */
switch (gpio_port >> 5) {
case 1: /* PORTA */
pctl = (PORT_MemMapPtr) PORTA_BASE_PTR;
break;
case 2: /* PORTB */
pctl = (PORT_MemMapPtr) PORTB_BASE_PTR;
break;
case 3: /* PORTC */
pctl = (PORT_MemMapPtr) PORTC_BASE_PTR;
break;
case 4: /* PORTD */
pctl = (PORT_MemMapPtr) PORTD_BASE_PTR;
break;
case 5: /* PORTE */
pctl = (PORT_MemMapPtr) PORTE_BASE_PTR;
break;
/* There is no possibility to get other port from table */
}
pctl->PCR[gpio_port & 0x1F] &= ~PORT_PCR_MUX_MASK; /* set pin's multiplexer to analog */
return IO_OK;
}
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------