1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1

1,606 Views
wyao75
Contributor I

1

0 Kudos
Reply
1 Reply

1,349 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi 姚 玮

I would suggest you change the default FTP server configuration to see whether it helps

In rtcs/source/include/rtcscfg.h

FTPSRVCFG_TX_BUFFER_SIZE: Size of the socket transmit buffer in bytes. This option cannot be overridden in runtime. The default value is 1460 bytes.

FTPSRVCFG_SEND_TIMEOUT: timeout value for server sockets in milliseconds, and cannot be changed during runtime. The default value is 500ms.

Regards

Daniel

0 Kudos
Reply