MQX Software Solutions Knowledge Base

cancel
Showing results for 
Search instead for 
Did you mean: 

MQX Software Solutions Knowledge Base

Discussions

Sort by:
Hi Community, Based on How to add RTCS to a Processor Expert Project Using KDS and KSDK​,  below you can find the steps to include MFS and Shell to a KDS3.0 project using KSDK1.2 and Processor Expert. Thank you Carlos_Musich for his great document and for providing the draft of this document. Regards, Isaac Avila
View full article
A new MQX Flash File System (FFS) add-on is available for Freescale MQX™ 4.0.2.   See MQX Downloads.  FFS provides wear-leveling support required for mapping MFS on top of NAND flash. Files available # Name Description 1 FSL_MQX__FFS_RELEASE_NOTES_4_0_2 Freescale   MQX™ FFS package 4.0.2 Release Notes 2 Freescale   MQX RTOS 4.0.2 FFS package NAND   Flash File System solution for MQX™ 4.0.2
View full article
This blog shares several issues reported by China customers when they use NAND FFS in MQX4.1.1. NAND FFS open failure issue Customer reported they can use a pressure test code to continuously open file, write file and close file, each time write about 20 bytes with append and they will find after running for a while, file open will fail and it returns error code 0x3067 (MFS_EOF). Each time file open failed, file has been written with 20480 bytes. This is a typical use case at customer side for data logging. The test code is attached named as "nand_pressure_test.cpp". Attached patch file named "mfs_write.patch" can resolve this issue. Memory allocation issue when using MFS & NAND FFS Customer run pressure test for MFS and NAND FFS by creating multiple levels of sub-folders (up to 100 levels) and in each sub-folder they create random number of files (up to 50). For each file, they will write 250 bytes. They found code failed to open new file when create sub-folders to 41 level. Traced the code on K70 tower and found actually this is not problem with MFS to search clusters for the new file, instead when the issue occurs, it's the drive_ptr (MFS_DRIVE_STRUCT) which is corrupted when MFS use memory allocation routine to allocate file path. The pressure test code for this case is attached. File named "MultiLevel_Folder_Test.zip". The memory corruption for MFS drive info is due to there is no protection in MFS_Parse_pathname() on whether the actual path name used passed from fopen will be exceeding 260 bytes which is fixed in mfs.h file to be compatible with Windows. So need to take care of this internal limitation when handling multiple level folders. MFS deadlock issue when using NAND FFS Customer reported random code block issue when running pressure test against NAND FFS. The issue is quite random, sometimes takes 12 hrs to reproduce the issue. Test code attached. Name is "MFS deadlock issue.zip". The resolution and description on this issue is in attached file named "MQX-4919 NandFFS explanation". Hao
View full article
Hi All, The new Freescale MQX™ 4.1.1 GA release is now available on www.freescale.com/mqxrtos ·          Files available           # Name Description 1 FSL_MQX_RELEASE_NOTES_4_1_1 Freescale   MQX™ RTOS 4.1.1 Release Notes 2 Freescale   MQX RTOS 4.1.1 for Linux This   release has the same basic code as the 4.1.1 version, with just the changes   needed to build and debug on Linux systems. 3 Freescale   MQX RTOS 4.1.1 MQX™    Source code. Includes an RTOS, File System, TCP/IP and USB host/device   software stacks. ·          What is New? ·          New Board Support Package o    FRDM-K64F o    TWR-K64F120M ·          New Features and Updates o    MQX RTOS 4.1.1 enables development on Linux machines o    MQX RTOS 4.1.1 supports the new Freescale IDE, Kinetis Design Studio o    Example ISR and related documentation is updated to give guidance on setting up a Kernel ISR (a.k.a Gorilla ISR) - extremely high priority ISR o    Power PC (PX) family support has been dropped o    Readme files are added to examples without a description o    Register definition header files for Kinetis MCUs are added for convenience when porting to an MCU sub-family device o    Both interrupt driven I2C master and slave mode drivers are changed to support synchronous blocking mode and share the same API with the polling driver variant.  Improves performance by eliminating the need to poll for data availability. ·          Known issues o    For known issues and limitations please consult the release notes
View full article
The Freescale MQX™ RTOS for Kinetis SDK FRDM-KL43Z Freescale Freedom Platform is now available on the www.freescale.com ·          Release Files             # Name Description 1                                   Freescale_MQX_KSDK_1.0.0-KL43Z.exe Windows installer. Freescale MQX™ RTOS software   components fully pre-integrated with the Kinetis SDK. Includes the MQX   kernel, USB host and device stacks, MFS file system, and example   applications. Does not require prior installation of Kinetis SDK. 2                                   Freescale_MQX_KSDK_1.0.0-KL43Z.bin Linux installer. Freescale MQX™ RTOS software   components fully pre-integrated with the Kinetis SDK. Includes the MQX   kernel, USB host and device stacks, MFS file system, and example   applications. Does not require prior installation of Kinetis SDK. 3 MQXKSDKKL43Z.pdf Freescale MQX™ RTOS for Kinetis   SDK FRDM-KL43Z Freescale Freedom Platform Release Notes ·          Target HW boards: o    Freescale Freedom FRDM-KL43Z platform with a MKL43Z256VLH4 processor ·          Key features:  o    PSP support for the MKL43Z256VLH4 Microcontroller o    BSP for the Freescale Freedom FRDM-KL43Z platform with a MKL43Z256VLH4 processor o    MQX STDLIB o    nShell o    KSDK Support for the MKL43Z256VLH4 Microcontroller o    MFS file system ·          Known issues For known issues and limitations please consult the release
View full article