vTaskdelay(), vTaskdelayuntil() call doesn't work on MPC5748G.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

vTaskdelay(), vTaskdelayuntil() call doesn't work on MPC5748G.

2,161件の閲覧回数
nirmal_kumar
Contributor I

vTaskdelay(), vTaskdelayuntil() call doesn't work on MPC5748G.

I created a project on Z0 core. -> Added freertos component via PE -> Generated the code.

On creating the task, it is successful.

But when i used vTaskdelay() inside the task, the application crashes. Removing the call woks fine.

I had to use vTaskdelay(), vTaskdelayUntil() in my application. 

I couldn't able to solve this. Kindly help.

Attached sample code.

ラベル(1)
0 件の賞賛
返信
1 返信

1,937件の閲覧回数
xierxiaofeng
Contributor II

Hi Nirmalkumar,

    Have you resolved this problem? I encountered the same problem.

Thannks!

0 件の賞賛
返信