tresos loading issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

tresos loading issue

3,662件の閲覧回数
bhavesh
Contributor II

I am trying to use MPC574XG_MCAL4_0_RTM_1_0_5 along with tresos, when I try to load configuration for it the following error is seen:

[Project: Calypso6M_MCAL4_0_sample_ap Plug-in with a module "Dem_TS_T2D35M10I3R0" is not installed - cannot create module configurations for project "Calypso6M_MCAL4_0_sample_ap"].

I think this error should not be there in the first place as all the plugins installer are of type xx_yy_abcd10I5R0, because i am using _1_0_5 version and not the _1_0_3.

I searched google for relevant problems but did not find any answer. Any help will be appreciated. 

Thank you.

0 件の賞賛
返信
2 返答(返信)

3,040件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

[Project: Calypso6M_MCAL4_0_sample_ap Plug-in with a module "Dem_TS_T2D35M10I3R0" is not installed - cannot create module configurations for project "Calypso6M_MCAL4_0_sample_ap"].

Is the sample application written and configured in 103 or 105?

If you create fresh configuration in 105 do you see any issues? (not sample app)

peter

0 件の賞賛
返信

3,040件の閲覧回数
netfish
Contributor I

I have the same issue, can anyone shed some light?

0 件の賞賛
返信