the bootloader jump function can not work in mpc5604P

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

the bootloader jump function can not work in mpc5604P

1,071 次查看
ananan
Contributor III

the jump function is nextpastedImage_1.png

the boot program is next,CODE_MAINADDR_START= 0x00008000(the APP org address);the code warrior warns No source available for "0x00000004 (0x00000004)() ; if CODE_MAINADDR_START= 0x00(the boot org address),the boot program jump to the boot program circulately,and it work well in the boot.

pastedImage_2.png

the APP link file is next

pastedImage_3.png

pastedImage_4.png

pastedImage_5.png

when I download the APP(org address is 0x00008000) using the code warrior 10.6,the APP program is work well.but the boot jump to the APP ,the code warrior warns the “source available for "0x00000004 (0x00000004)()””。I really do not how to it and can not get the issue about the problem. please help me ,I  warry it a lot !

0 项奖励
回复
0 回复数