questions about Static library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

questions about Static library

1,054件の閲覧回数
William-Lee
Contributor II

一、There are three project files in the PJ folder:

  • MPC5748G_RTM300_S32DS21_sourcecodes_Z4_0:Source codes project.
  • MPC5748G_RTM300_S32DS21_createlibrarycodes_Z4:Packaging static library project.
  • MPC5748G_RTM300_S32DS21_uselibrary_Z4_0:use the static library project.

 

二、procedure description:

I buid a new application project and named

“MPC5748G_RTM300_S32DS21_sourcecodes_Z4_0”. In this project , I add timing_pal1 to ProcessorExperts , and configure PIT channel 0 as delay function. The final codes is ok.But when I packaging it to a library project and use it in another application project ,it did not work. Can you teach me what went wrong? I will upload the three projects ,thanks for your help!

WilliamLee_0-1656487266215.png

 

WilliamLee_1-1656487266633.png

 

 

0 件の賞賛
返信
0 返答(返信)