Erros happened in libyary invoking based on MPC5748G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Erros happened in libyary invoking based on MPC5748G

381 Views
Eric_Chen99
Contributor II

the function of delay is verified in an application project, and this function is sealed in a library file (xxx.a), when invoke the delay function of the  library in another application project,  the  project process  is   lost. please see the figure: by the way, invoke other initialization functions in the library, the project  is ok, perhaps the interrupts problems of the delay function .  

 

 

图片1.png

Tags (1)
1 Reply

364 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

how is the delay function implemented? It is possible that in previous project it uses some already configured timer or whatever, but in the new project is not this peripheral initialized or already taken by other functionality. 

0 Kudos