problem with compiling MPC574XP_MCAL4_0_RTM_2_0_2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem with compiling MPC574XP_MCAL4_0_RTM_2_0_2

Jump to solution
6,426 Views
Ehsaaan
Contributor III

Hello
I am going to compile the MPC574XP_MCAL4_0_RTM_2_0_2 example with the makefile by launching launch.bat , but I got an error:


make (e=2) : the system cannot find the file specified.
make.exe: *** [Adc.o] Error 2

Could anybody help?

Tags (1)
0 Kudos
Reply
1 Solution
6,419 Views
hungnguyenphi
NXP Employee
NXP Employee

Hello @Ehsaaan ,

 

Could you please check if you have filled the correct value for the MAKE_DIR, TRESOS_DIR, ... in the launch.bat file. Eg:

hungnguyenphi_0-1632303478757.png

 

 

Best regards,

Hung

View solution in original post

6 Replies
6,352 Views
hungnguyenphi
NXP Employee
NXP Employee

Hello @Ehsaaan ,

 

Have you resolved the configuration issue. If not could you please share your EB project or at least the Mcu configuration(.xdm or .epc). Then I will check it.

 

Best regards,

Hung

0 Kudos
Reply
6,380 Views
Ehsaaan
Contributor III

Also, in the file of this example, running launch.bat without any changes, I encounter these errors:

0 Kudos
Reply
6,356 Views
namnguyenviet
NXP Employee
NXP Employee

You should try with the compiler version mentioned in the Release note:

namnguyenviet_0-1632713818362.png

 

The newer version might update some features which MCAL were not verified with.

Best Regards,

Nam

 

0 Kudos
Reply
6,420 Views
hungnguyenphi
NXP Employee
NXP Employee

Hello @Ehsaaan ,

 

Could you please check if you have filled the correct value for the MAKE_DIR, TRESOS_DIR, ... in the launch.bat file. Eg:

hungnguyenphi_0-1632303478757.png

 

 

Best regards,

Hung

6,397 Views
Ehsaaan
Contributor III

Hello.
@hungnguyenphi 
Yes, that problem is solved now, I set the compiler direction wrong.
But now I have some new problems... 
the error log and other info are attached here.

0 Kudos
Reply
6,346 Views
hungnguyenphi
NXP Employee
NXP Employee

Hello @Ehsaaan ,

 

Could you please share your EB project of the Mcu configuration file(.xdm or .epc file).Then I will check it.

 

Best regards,

Hung

0 Kudos
Reply