Hi,
I was looking for documentation about the PowerPC cores in the MPC5777M (e200z710n3 / e200z425Bn3) to set up eg the internal timebase register and decrement counter, check other SFRs, ...
I found these two
e200z446n3
https://www.nxp.com/docs/en/reference-manual/e200z4RM.pdf
e200z760n3
https://www.nxp.com/docs/en/reference-manual/e200z760RM.pdf
but not ones exactly for the e200z710n3 or e200z425Bn3 - are the z446 and z760 close enough to be useful? Is there more specific documents for the other cores?
Thanks,
Jacob
已解决! 转到解答。
Unfortunately, core reference manuals only exist for core variants used on MPC55xx/56xx devices.
Core variants used with MPC57xx devices are only described in MPC57xx device reference manuals. For instance, MPC5777MRM, specifically in chapters 13-15.
Following documents exist comparing cores to each other:
http://www.nxp.com/files/microcontrollers/doc/app_note/AN4802.pdf
Also following presentation could be useful:
http://www.nxp.com/files/training/doc/ftf/2014/FTF-AUT-F0345.pdf
In case specific details is needed to consult, please create new case and we’ll try to help you:
https://community.nxp.com/docs/DOC-329745I was looking for full information on the e200z425 core also. I've been able to be sure exactly what assembler opcodes it supports for floating point maths. Is there a definitive reference that tells me exactly which instructions are available?
I also found that the S32DS compiler is emitting opcodes that do not appear to be listed in the VLE documents.
Confused!
James
Following 3 documents should cover all opcodes:
http://www.nxp.com/files/32bit/doc/ref_manual/EREF_RM.pdf
http://www.nxp.com/files/32bit/doc/ref_manual/VLEPEM.pdf
http://www.nxp.com/files/32bit/doc/ref_manual/SPEPEM.pdf
However they may be some unsupported instructions for specific core variants.
Unfortunately, core reference manuals only exist for core variants used on MPC55xx/56xx devices.
Core variants used with MPC57xx devices are only described in MPC57xx device reference manuals. For instance, MPC5777MRM, specifically in chapters 13-15.
Following documents exist comparing cores to each other:
http://www.nxp.com/files/microcontrollers/doc/app_note/AN4802.pdf
Also following presentation could be useful:
http://www.nxp.com/files/training/doc/ftf/2014/FTF-AUT-F0345.pdf
In case specific details is needed to consult, please create new case and we’ll try to help you:
https://community.nxp.com/docs/DOC-329745