MPC5746R-176DS does not come out of reset

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5746R-176DS does not come out of reset

跳至解决方案
738 次查看
folkertsikkema
Contributor II

Dear,

I just received my new bought set of motherboard, MPC5746R-176DS and PE Multilink FX
and want to start playing. Big thing seems to be: the board is not coming out of reset. Both
the red LEDs for Reset and Porst stay on. In fact: I do not know if that is correct, but the
debugger does not want to make any connection with the target (but the yellow "i am connected
to the target" LED is lit).

I also tried to PROGPPCNEXUS from PEMicro but that one is also not able to make a
connection with my board.

Is there anyone out here who can push me in the right direction?

Regards, Folkert

ps: S32 gives various error codes...

标记 (1)
1 解答
637 次查看
folkertsikkema
Contributor II

Finally it turns out that one of the jumpers was not in the correct default position.

在原帖中查看解决方案

1 回复
638 次查看
folkertsikkema
Contributor II

Finally it turns out that one of the jumpers was not in the correct default position.