mpc8247 scc controller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mpc8247 scc controller

1,602件の閲覧回数
1174498516
Contributor I

Our development board for MPC 8247, the SCC controller is set to network mode interrupt can trigger, but set to serial mode interrupt can not trigger, but SCC set to serial mode polling mode is good. Why is that?

0 件の賞賛
返信
2 返答(返信)

1,516件の閲覧回数
Pavel
NXP Employee
NXP Employee

See attached files. These files are simple SCC HDLC and transparent example using interrupt.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,516件の閲覧回数
1174498516
Contributor I

OK,thanks

发自我的iPhone

0 件の賞賛
返信