mpc8247 scc controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mpc8247 scc controller

1,607 Views
1174498516
Contributor I

Our development board for MPC 8247, the SCC controller is set to network mode interrupt can trigger, but set to serial mode interrupt can not trigger, but SCC set to serial mode polling mode is good. Why is that?

0 Kudos
Reply
2 Replies

1,521 Views
Pavel
NXP Employee
NXP Employee

See attached files. These files are simple SCC HDLC and transparent example using interrupt.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,521 Views
1174498516
Contributor I

OK,thanks

发自我的iPhone

0 Kudos
Reply