mpc5748g EEE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mpc5748g EEE

Jump to solution
2,488 Views
skseofh
Contributor II

Hi, I'm using mpc5748G EEE module.

 

I'm trying to use same block and seperates into 2 blocks like this.

*Mid space block 0 : start address - 0x00F90000, end address - 0x00F93FFF, size - 16KB

 - block configuration 0 : start address - 0x00F90000, size - 0x00002000

 - block configuration 1 : start address - 0x00F92000, size - 0x00002000

skseofh_1-1631161629800.png

 

It works on 'Init, Write, Read, Delete' SDK function, but it's not working on 'EEE_DRV_ReportEepromStatus()' function.

Is it not possible to use like this?

0 Kudos
Reply
1 Solution
2,474 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

no, this will not work. Those blocks must correspond to physical blocks. The smallest portion of flash which we can erase is one block. It is not possible to erase only one half of such block. That means the driver will definitely fail.

Please keep the blocks aligned with physical blocks.

Regards,

Lukas

View solution in original post

0 Kudos
Reply
1 Reply
2,475 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

no, this will not work. Those blocks must correspond to physical blocks. The smallest portion of flash which we can erase is one block. It is not possible to erase only one half of such block. That means the driver will definitely fail.

Please keep the blocks aligned with physical blocks.

Regards,

Lukas

0 Kudos
Reply