mpc5643l Rappid bootloader error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mpc5643l Rappid bootloader error

2,020 次查看
satvicky
Contributor I

Hello,

I am getting an error saying BAM communication loss with MPC564xL, with reason as BAM Password check or FAB, ABS2, ABS0 settings check.

I am using FAB = 1, ABS2 = 1, ABS0 = 0 setting ( FlexCAN with autobaud feature )

Password is the default one : 0xFEEDFACECAFEBEEF

Any hints where am i going wrong with my settings ?

Thanks.

标签 (1)
0 项奖励
回复
3 回复数

1,889 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I have not run into any problems using the EVB.  I just ran it 10 times with just hitting the reset when prompted by the bootloader with no issue.  To run the bootloader for MPC5643L I usually have the FAB and ABSx pins setup for Auto Baud or FAB = 1, ABS0 = 0 and ABS2 = 1.

I also took a picture of the board that I am using so that you can see my jumper settings.

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

Regards,

Lukas

0 项奖励
回复

1,889 次查看
satvicky
Contributor I

Hi Lukas,

Thanks for the reply.

You say you have kept the following settings :

FAB = 1 = ABS2, ABS0 = 0. This is for FlexCAN autobad feature and as i read in the manual, MPC5643L chip doesnt support FlexCAN autobad. It only supports : SCI(FAB = 1,  ABS2 = ABS0 = 0) and serial CAN(FAB = 1 = ABS0, ABS2=0)

Also you have made serial port as connection medium, though you selected FlexCAN.

Can you please throw some light onto this, how it is working for you ?

Thanks!!

0 项奖励
回复

1,889 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

cut2/3 supports autobaud feature.

Page 193:

pastedImage_2.png

Page 195:

pastedImage_1.png

Regards,

Lukas

0 项奖励
回复