mpc5554 strange error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mpc5554 strange error

3,642 Views
juzi
Contributor I
 
 hi,
when i debug an empty project created follow the cw wizard,it works ok(flash mode), 
 but when i change the code start address
internal_flash:       org = 0x00020000,   len = 0x00060000 
in -flash.clf.         it does not work,can you tell me why? it is an empty project, i do not
add any user code.
for example  i change org = 0x00020000  to another address org = 0x00100000, it can not work.   it always reset.  and can you tell me why? can you tell me something about how to change my code start address? 
the tools i use are P&E powerpc nexus debugger,codewarrior for mpc55xx V2.2 and Axiom MPC5554evb board .
thanks, regards
 
Labels (1)
0 Kudos
Reply
1 Reply

2,847 Views
EAlepins
Contributor V
Hi,
 
Just an idea : did you check the option Settings->Linker->EPPC Linker->Generate ROM Image? There are two text box there : RAM Buffer Address and ROM Image Address.
 
I had problem when I activated that. It forced me to have a ROM application. I also suppose that this address must match that of your lcf.
 
Étienne
0 Kudos
Reply