linking with no compile in AUTOSAR samples from NXP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

linking with no compile in AUTOSAR samples from NXP

1,900 Views
Ehsaaan
Contributor III

Hello Dears,

Assume that we have the .O files(objects) after compiling. now I wanna linking the .O files with no compiling the sources again. just linking the .o files. apparently, I should do this if possible by modifying the content of makefiles. could anyone help??\

I am speaking about NXP's AUTOSAR sample projects in the site. e.g. MPC574XG_MCAL4_0_RTM_1_0_5_Sample_Application\ and the make files inside it...

0 Kudos
Reply
4 Replies

1,857 Views
namnguyenviet
NXP Employee
NXP Employee

Hello,

It will not be easy to archive that in Makefile, cause the OUT_FILES variable depends on the source files (.c, .C and .s files) which could be found by Make GNU. Without the knowledge of these files, there will be no object file acknowledged, hence the Makefile will not include the object files without a source file as reference.

You can use the command to link the object files, for example:

C:/ghs/comp_201914/ccppc.exe -cpu=ppc5748gz4204 -vle -nostartfiles --nocpp -Mn -delete -ignore_debug_references -keepmap ./toolchains/autosar_flash.ld ./bin/Adc.o  [...] ./bin/sample_app_mcal_task_1.o ./bin/sample_app_mcal_task_2.o ./bin/sample_app_mcal_task_3.o ./bin/sample_app_mcal_uart_console.o -o bin/sample_app_mcal.elf

(list out all of the object files and paths in [...])

Best Regards,

Nam

 

 
0 Kudos
Reply

1,873 Views
Ehsaaan
Contributor III

Can anybody help with this topic???

0 Kudos
Reply

1,890 Views
namnguyenviet
NXP Employee
NXP Employee

Hello,

It's a makefile dependencies topic: basically, if there is no change within dependencies of a target, then that target will not be touched. For instance, in a make environment, if you didn't change any object files, which are dependencies of an elf file, then that elf file will not be re-created; or when you modify one source file, only the object for that source file is re-created (not all of the objects are re-created). Here you can find some useful information about it:

https://www.tutorialspoint.com/makefile/makefile_recompile.htm

The sample application in MPC574xG_MCAL4_0_RTM_1_0_5 has already supported this. 

Best Regards,

Nam

 

0 Kudos
Reply

1,880 Views
Ehsaaan
Contributor III

Thank You, Dear Nam.
But my main question is:
Assume that I just had the .O files here. somebody did the compilation on another computer and gave me just the .O files. And now I wanna make a .elf file from this .O files. there's no .C/.CPP files are available to compile. ok? 

0 Kudos
Reply