init      Linker Generated Symbol File

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

init      Linker Generated Symbol File

2,059 Views
wanglong
Contributor II

在rom.map没有这个是为什么?

Labels (1)
4 Replies

1,908 Views
wanglong
Contributor II

Boot Assist Module (BAM) with FlexCAN MPC5534

Hello !

I need to use the Boot Assist Module to boot an application from FlexCan bust to internal SRAM.

 I  modify the start.c,but my rom.mot is not use.

Can help me with a example code? Just I have to modify the Linker Files?

Thank you very much for your time!

0 Kudos
Reply

1,908 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Please do not duplicate the threads. Follow https://community.nxp.com/thread/443190 

0 Kudos
Reply

1,908 Views
wanglong
Contributor II

Hi, I met a problem when I was using mpc5634, and I generated ram.mot files on the way you provided, but my application didn't run on ram! What's the reason? Can help me? Thank you for your。

0 Kudos
Reply

1,908 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

at first, could you please write your question in English? Second, the question does not make any sense to me. Could you please clarify it?

Regards,

Martin