how to solve high voltage appearring after reset until init code about MPC5744P

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to solve high voltage appearring after reset until init code about MPC5744P

1,959 Views
jinhui_wu
Contributor III

Due to Weak up-pull resister of GPIO pin,there will be a high level voltage apperring.

because i use the GPIO to drive a high-side IC and high level is an active level.

Therefor,after mcu reset,the GPIO appear high level until GPIO init fuction.

the high level will effect the high-side IC,this may result in some error in my board.

How to solve high voltage?

Labels (1)
Tags (1)
2 Replies

1,858 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

You have to apply external pull down on this GPIO.

There is no possibility to reconfigure this other then in application SW.

Peter

1,858 Views
jinhui_wu
Contributor III

What's the mean of "There is no possibility to reconfigure this other then in application SW."

if i apply external pull down resister.what's the value of resister do you suggest?

if i pull down 5kOhm,does the GPIO have 1V voltage?

0 Kudos
Reply