how to import CodeWarrior Development Studio V2.10 project in CodeWarrior 11.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to import CodeWarrior Development Studio V2.10 project in CodeWarrior 11.1

2,011 次查看
liyue1
Contributor I

I use the cw 2.10 in windows 7, but it can not use in windows 10 ,so I need to upgrade version 11.1 in windows 10,but i do not  want to add by one of one source.I want to import project quickly.Please  help me ?

0 项奖励
回复
2 回复数

1,979 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I haven;t tried it but there is guide for porting classic to eclipse:

https://www.nxp.com/docs/en/application-note/AN4727.pdf

petervlna_0-1700468487943.png

 

@stanish Can you comment here?

Best regards,

Peter

0 项奖励
回复

1,940 次查看
stanish
NXP Employee
NXP Employee

Hello, 

There indeed used to be a CodeWarrior Classic project importer in CodeWarrior for MCU (eclipse based).

It was removed prom the product quite some time ago due to its limitations. Anyway If you'd like to try it you can download and install CodeWarrior v10.2 where it should be still available and try to migrate your project.

Anyway you can always create a dummy project in the latest version of CW for MCUs and copy your existing source files into new project, adjust the .h file paths, adjust the tools settings (see attached document) to match with your original project and copy linker file.  Such a project will already include debug configurations.

Hope it helps.

Stan

0 项奖励
回复