failed when debugging ethernet_UDP example project in S32 Design Studio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

failed when debugging ethernet_UDP example project in S32 Design Studio

1,561件の閲覧回数
yachuanliu
Contributor II

Hello all, a problem occurred when I debug the enet_rmii_udp project in MPC5748G from the S32 Design Studio example. I can’t debug the project successfully. The pictures below are the errors showed in S32 console tab when debugging this project.

 error.PNG

error0.PNGerror1.PNG

Here are some other message you may need.

  1. S32 version: S32 Design Studio for Power Architecture v1.2.
  2. The enet_rmii_udp project: imported from S32DS Example Projects. And I didn’t change anything.捕获.PNG
  3. I debugged the hello example project successfully using the same computer, same MPC5748G.

I really need your help. Thanks.

1 返信

1,414件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

I handle this issue in the thread below:

https://community.nxp.com/thread/470701?sr=inbox 

Regards,

Martin