failed when debugging ethernet_UDP example project in S32 Design Studio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

failed when debugging ethernet_UDP example project in S32 Design Studio

1,528 Views
yachuanliu
Contributor II

Hello all, a problem occurred when I debug the enet_rmii_udp project in MPC5748G from the S32 Design Studio example. I cant debug the project successfully. The pictures below are the errors showed in S32 console tab when debugging this project.

 error.PNG

error0.PNGerror1.PNG

Here are some other message you may need.

  1. S32 version: S32 Design Studio for Power Architecture v1.2.
  2. The enet_rmii_udp project: imported from S32DS Example Projects. And I didnt change anything.捕获.PNG
  3. I debugged the hello example project successfully using the same computer, same MPC5748G.

I really need your help. Thanks.

1 Reply

1,381 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

I handle this issue in the thread below:

https://community.nxp.com/thread/470701?sr=inbox 

Regards,

Martin