error during Flash programming 5777C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

error during Flash programming 5777C

3,416件の閲覧回数
San_96
Contributor I

I am unable to dump program to the card.

MPC5777C controller,

S32DS V1.2 IDE

PE micro USB multilink

While I try to dump the program, the below error is shown.

Initializing.
MPC577xC Device detected.
Target has been RESET and is active.
CMD>CM C:\NXP\S32DS_Power_v1.2\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.6.7.201706090048\win32\gdi\P&E\nxp_mpc5777c_1x32x2048k_cflash_highspeed.pcp

Initializing.
MPC577xC Device detected.
Initialized.

;version 1.04, 12/13/2016, Copyright P&E Microcomputer Systems, www.pemicro.com [5777C_8meg_highspeed]

;device NXP, MPC5777C, 1x32x2048k, desc=CFlash_highspeed

;begin_cs device=$30800000, length=$00800000, ram=$00300000
Loading programming algorithm ...
Error loading .PCP file : C:\NXP\S32DS_Power_v1.2\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.6.7.201706090048\win32\gdi\P&E\nxp_mpc5777c_1x32x2048k_cflash_highspeed.pcp at address 00300001
Error loading programming algorithm - load aborted.
Error occurred during Flash programming. 

And then Starting reset script.....

After some time, one error pop-up is shown as Flash programming error. terminating debug session.

The PE micro multilink and S32DS V1.2 IDE, I use, works well with other cards with MCU 5567, 5777. With this card only it is showing error. I checked all hardware connections. Everything is perfect as I designed the previous cards. With this card, things are not at all moving further. Need help.

0 件の賞賛
返信
5 返答(返信)

3,396件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I've never seen this issue before.

1. Please check if the nxp_mpc5777c_1x32x2048k_cflash_highspeed.pcp file is in the specified folder.

2. Please update the PEMicro plugin.

Best regards,

Peter

0 件の賞賛
返信

3,393件の閲覧回数
San_96
Contributor I

Hi,

I checked the file. It is there in path. 

PEmicro is working properly for other project cards of MPC5777C same batch

0 件の賞賛
返信

3,373件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

What comes to my mind. I sometimes have issue programming SPC5777C when its flash it is not erased first. Try to erase flash, once it is cleared, program it.

Best regards,

Peter

0 件の賞賛
返信

2,687件の閲覧回数
IvanIvanenkoTechSAT
Contributor II

Hello.
I have exactly the same problem.
S32 design studio, PE plugin and Multilink firmware are up-to-date.
Was any solution founded last time?

0 件の賞賛
返信

2,670件の閲覧回数
San_96
Contributor I
Hi,
At that time, we have given 5V to a pin instead of 3.3V. So, that caused problem when trying to program the code. Later, we verified the supply levels to all pins and rectified our mistake. After that, this issue is resolved.
But, sometimes, I get this error during flash programming, due to improper/loose connection of PE device cable / power supply not enough..
0 件の賞賛
返信