eptu_cw code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eptu_cw code

2,204件の閲覧回数
xiaojin
Contributor I

I download etpu code form

http://www.nxp.com/webapp/etpu_cw/

I want to use GPIO/IC/OC/PWM functions, but only the GPIO function are ok, the IC/OC/PWM functions doesn't work.

I find that the IC/OC/PWM api interface is not up to date, can you provide me the etpu api which is suitable for etpu_cw funcitons?

タグ(1)
0 件の賞賛
返信
1 返信

1,909件の閲覧回数
MilanBrejl
NXP Employee
NXP Employee

Correct API for OC, IC, PWM (PowerPC version) is now up on the Function Selector. Please create the function set and download again.
-Milan

0 件の賞賛
返信