eTimer Module questions of MPC5744P

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

eTimer Module questions of MPC5744P

跳至解决方案
2,138 次查看
qm1013
Contributor III

HI, I have a question about the eTimer module , I use the eTimer module to measure PWM signal, to measure the frequency ,period , pulseH and pulseL ,.

here is the questions:

1. If I set ONESHOT bit to 0, which means that the counter is in free running mode, will the capture still continue when the ICF2/1 (Input Capture 2/1 Flag) is set ?

2. If I set ONESHOT bit to 1, which menas that the counter is  one shot capture mode , and i still set the CFWM(Capture FIFO Water Mark) to 1 , will the capture register to capture twice before the ICF2/1 (Input Capture 2/1 Flag) is set ?

Regards,

meng

标记 (2)
0 项奖励
回复
1 解答
1,969 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

1. If I set ONESHOT bit to 0, which means that the counter is in free running mode, will the capture still continue when the ICF2/1 (Input Capture 2/1 Flag) is set ?

Yes

2. If I set ONESHOT bit to 1, which means that the counter is  one shot capture mode , and i still set the CFWM(Capture FIFO Water Mark) to 1 , will the capture register to capture twice before the ICF2/1 (Input Capture 2/1 Flag) is set ?

When ONESHOT is set to 1, eTimer is waiting for one edge and then it is stole.

When watermark is set to 1, flag is set after second edge. But the second edge will occur only if you again start capture via ARM bit, because you have one shot mode.

regards,

Peter

在原帖中查看解决方案

1 回复
1,970 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

1. If I set ONESHOT bit to 0, which means that the counter is in free running mode, will the capture still continue when the ICF2/1 (Input Capture 2/1 Flag) is set ?

Yes

2. If I set ONESHOT bit to 1, which means that the counter is  one shot capture mode , and i still set the CFWM(Capture FIFO Water Mark) to 1 , will the capture register to capture twice before the ICF2/1 (Input Capture 2/1 Flag) is set ?

When ONESHOT is set to 1, eTimer is waiting for one edge and then it is stole.

When watermark is set to 1, flag is set after second edge. But the second edge will occur only if you again start capture via ARM bit, because you have one shot mode.

regards,

Peter