eTimer Module questions of MPC5744P

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eTimer Module questions of MPC5744P

ソリューションへジャンプ
2,142件の閲覧回数
qm1013
Contributor III

HI, I have a question about the eTimer module , I use the eTimer module to measure PWM signal, to measure the frequency ,period , pulseH and pulseL ,.

here is the questions:

1. If I set ONESHOT bit to 0, which means that the counter is in free running mode, will the capture still continue when the ICF2/1 (Input Capture 2/1 Flag) is set ?

2. If I set ONESHOT bit to 1, which menas that the counter is  one shot capture mode , and i still set the CFWM(Capture FIFO Water Mark) to 1 , will the capture register to capture twice before the ICF2/1 (Input Capture 2/1 Flag) is set ?

Regards,

meng

タグ(2)
0 件の賞賛
返信
1 解決策
1,973件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

1. If I set ONESHOT bit to 0, which means that the counter is in free running mode, will the capture still continue when the ICF2/1 (Input Capture 2/1 Flag) is set ?

Yes

2. If I set ONESHOT bit to 1, which means that the counter is  one shot capture mode , and i still set the CFWM(Capture FIFO Water Mark) to 1 , will the capture register to capture twice before the ICF2/1 (Input Capture 2/1 Flag) is set ?

When ONESHOT is set to 1, eTimer is waiting for one edge and then it is stole.

When watermark is set to 1, flag is set after second edge. But the second edge will occur only if you again start capture via ARM bit, because you have one shot mode.

regards,

Peter

元の投稿で解決策を見る

1 返信
1,974件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

1. If I set ONESHOT bit to 0, which means that the counter is in free running mode, will the capture still continue when the ICF2/1 (Input Capture 2/1 Flag) is set ?

Yes

2. If I set ONESHOT bit to 1, which means that the counter is  one shot capture mode , and i still set the CFWM(Capture FIFO Water Mark) to 1 , will the capture register to capture twice before the ICF2/1 (Input Capture 2/1 Flag) is set ?

When ONESHOT is set to 1, eTimer is waiting for one edge and then it is stole.

When watermark is set to 1, flag is set after second edge. But the second edge will occur only if you again start capture via ARM bit, because you have one shot mode.

regards,

Peter