eTPU question about RPM.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eTPU question about RPM.

1,662 Views
DooDo
Contributor I

Hi,

The S32 DS uses the engine control eTPU of the MPC5777.

I set it up as below.

#define SYS_FREQ_HZ 160E6
#define TCR1_FREQ_HZ (SYS_FREQ_HZ/2)
#define TEETH_TILL_GAP 58
#define TEETH_IN_GAP 2
#define TEETH_PER_CYCLE 120
#define TCR2_TICKS_PER_TOOTH 600 //  600 1000
#define TCR2_TICKS_PER_CYCLE ((TEETH_PER_CYCLE)*(TCR2_TICKS_PER_TOOTH))
#define MSEC2TCR1(x) (TCR1_FREQ_HZ/1E3*(x)/1E0)
#define USEC2TCR1(x) (TCR1_FREQ_HZ/1E3*(x)/1E3)
#define NSEC2TCR1(x) (TCR1_FREQ_HZ/1E3*(x)/1E6)
#define DEG2TCR2(x) ((x)*TCR2_TICKS_PER_CYCLE/720) 
#define UFRACT24(x) ((x)*0xFFFFFF)

I put the RPM in 3000 and made it work. I understand that RPM is the same as crank rotation for 1 minute, but the crank frequency came out to be about 25Hz.

RPM = 25Hz * 60 = 1500 Half of what RPM put in.

How am I supposed to understand?

#define TCR1_FREQ_HZ (SYS_FREQ_HZ/2)

I don't know why this is TCR1 half of SYS. In the AN4908 example, it was a one-to-one ratio.

I don't know a lot because I received the completed project.

 

0 Kudos
Reply
2 Replies

1,651 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

With eTPU2 it can be 1:1 ratio, but eTPU uses 1:2 ratio.

Example code apparently uses backward compatible code

davidtosenovjan_1-1693299468195.png

 

davidtosenovjan_0-1693299426894.png

davidtosenovjan_2-1693299716552.png

 

 

0 Kudos
Reply

1,612 Views
DooDo
Contributor I

Thank you,

I set the RPM, but the RPM comes out in half. What's wrong?

#define RPM2TP(x) (TCR1_FREQ_HZ/(x)*60/(TEETH_PER_CYCLE/2))

I put the value through RPM2TP, is the above definition wrong?

0 Kudos
Reply