eMIOS Register Access

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eMIOS Register Access

ソリューションへジャンプ
2,715件の閲覧回数
Bobkat
Contributor II

Hi,

Is there a way I can access  eMIOS registers, e.g. eMIOS_0.MCR_B.GPREN etc... in addition to using one of the SDKs.

I need low-frequency pwm (50-200Hz) for the application and have been advised to avoid using the SDK for this purpose.

I've managed to get the code working based on one of the emios example projects.

The problem I'm encountering is that if I've configured the project to use one of the SDKs (SDK_S32_PA_15), as soon as I include 'project.h' for the emios code as is required by the example , I get a mass of errors related to redefinition of variables etc. If I remove 'project.h' in favour of 'Cpu.h', the compiler can't find the register definition I need for configuration.

I would greatly appreciate any help on this matter.

 

Best regards

 

Rob

0 件の賞賛
返信
1 解決策
2,702件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, you can access eMIOS registers in SDK code too. Just follow registers definition in respective header file. So you can have e.g. 

eMIOS_0->MCR |= eMIOS_MCR_GPREN(1);
eMIOS_0->MCR |= eMIOS_MCR_GPREN_MASK

BR, Petr

元の投稿で解決策を見る

2 返答(返信)
2,703件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, you can access eMIOS registers in SDK code too. Just follow registers definition in respective header file. So you can have e.g. 

eMIOS_0->MCR |= eMIOS_MCR_GPREN(1);
eMIOS_0->MCR |= eMIOS_MCR_GPREN_MASK

BR, Petr

2,678件の閲覧回数
Bobkat
Contributor II

Sorry for the late reply.

 

Cheers Petr.

 

Best regards

Rob

0 件の賞賛
返信