eMIOS OPWMB mode Query

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

eMIOS OPWMB mode Query

1,738 次查看
atuldixit
Contributor I

I am using MPC5746C for my project development.

eMIOS 0 channels uses as per project requirement:

Channel : 0,8,16,22,23,24 (Type X ), (1,2,3,4,5,6) (Type G ) using OPWFMB

Channel : 20,21,26,26,28,29,30,31 (Type Y) using OPWMB

Channel : 9,10,11,12,13,14 (Type H)  using IPM

For using OPWMB mode, external counter is required and user need to configure external counter via MCB mode. That external counter is the time base to operate PWM channel for 20,21,26,26,28,29,30,31.

Now as per project requirement if each channel has a different frequency, then how to handle this situation because almost all channel has been used and hardware design in fixed?

标记 (1)
0 项奖励
回复
1 回复

1,594 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi Atul,

no way. The freq/period of OPWMB channels is given by its Counter Bus, as you wrote. If you need different freq then OPMFMB must be used.

BR, Petr.

0 项奖励
回复