dual core ${ProjDirPath} command issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

dual core ${ProjDirPath} command issue

1,852件の閲覧回数
supra0309
Contributor I

Hi:

I'm using 5746R to accomplish dual core function. Referenced from example s32r274_shmem_S32DS_Power_v1.2(https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/Example-S32R274-multi-core-shared-memo... I found there's a linker setting in s32r274_shmem_Z7_1. But I can't figure out the detail shows in "${ProjDirPath}/../s32r274_shmem_Z7_0/Debug/src/shared_mem.o" which is hidden with "..". Please tell me the detailed description. Thanks.

BR,

Xantia

supra0309_0-1676342382325.png

 

0 件の賞賛
返信
3 返答(返信)

1,831件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Correct me if I am wrong, but are you asking me what is the full path of "shared_mem.o" located at your PC machine?

Best regards,

Peter

0 件の賞賛
返信

1,827件の閲覧回数
supra0309
Contributor I

Hi:

I'm not sure what it means in this item. I tried to point it to workspace folder on my PC, but system showed some header files "No such file or directory" in core z4_1 project which are assigned in core z4_0 project.

How should I fix it, thanks

BR,

Xantia

0 件の賞賛
返信

1,820件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Either copy requested header files to the path you have set in config

or edit path properties to point in the location where you have that file.

Best regards,

Peter

0 件の賞賛
返信