dual core ${ProjDirPath} command issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

dual core ${ProjDirPath} command issue

1,885 Views
supra0309
Contributor I

Hi:

I'm using 5746R to accomplish dual core function. Referenced from example s32r274_shmem_S32DS_Power_v1.2(https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/Example-S32R274-multi-core-shared-memo... I found there's a linker setting in s32r274_shmem_Z7_1. But I can't figure out the detail shows in "${ProjDirPath}/../s32r274_shmem_Z7_0/Debug/src/shared_mem.o" which is hidden with "..". Please tell me the detailed description. Thanks.

BR,

Xantia

supra0309_0-1676342382325.png

 

0 Kudos
Reply
3 Replies

1,864 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Correct me if I am wrong, but are you asking me what is the full path of "shared_mem.o" located at your PC machine?

Best regards,

Peter

0 Kudos
Reply

1,860 Views
supra0309
Contributor I

Hi:

I'm not sure what it means in this item. I tried to point it to workspace folder on my PC, but system showed some header files "No such file or directory" in core z4_1 project which are assigned in core z4_0 project.

How should I fix it, thanks

BR,

Xantia

0 Kudos
Reply

1,853 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Either copy requested header files to the path you have set in config

or edit path properties to point in the location where you have that file.

Best regards,

Peter

0 Kudos
Reply