complete SPI driver code (including all api  with functionalities) for MPC5744p

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

complete SPI driver code (including all api  with functionalities) for MPC5744p

2,825件の閲覧回数
padmalathagudip
Contributor I

Hello ALL,

 

Iam working on MPC5744P evalutiona board, In that iam trying to implement the complete SPI driver code  with all api' s like  spi_init, SPI_send, SPI_receive, SPI_clockPolarity, SPI_CLockphase,SPI_baudratechange etc , SPI is having 4 ports (SPI0,SPI1,SPI2, SPI3),so we need to selct all ports anf need to inplement in such way that to set all clock, polarity, phase, baudrate, tranfer,  SO Please can you  provide the complete SPI driver code (including all API's with complete functinality) for MPC5744P ?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,255件の閲覧回数
Pat
Contributor III
0 件の賞賛
返信

2,255件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

We offer such complete driver.

You can find it on our web site here:AUTOSAR Software Solutions|NXP

But be aware that it is not free of charge.

Peter

0 件の賞賛
返信