complete SPI driver code (including all api  with functionalities) for MPC5744p

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

complete SPI driver code (including all api  with functionalities) for MPC5744p

2,818 Views
padmalathagudip
Contributor I

Hello ALL,

 

Iam working on MPC5744P evalutiona board, In that iam trying to implement the complete SPI driver code  with all api' s like  spi_init, SPI_send, SPI_receive, SPI_clockPolarity, SPI_CLockphase,SPI_baudratechange etc , SPI is having 4 ports (SPI0,SPI1,SPI2, SPI3),so we need to selct all ports anf need to inplement in such way that to set all clock, polarity, phase, baudrate, tranfer,  SO Please can you  provide the complete SPI driver code (including all API's with complete functinality) for MPC5744P ?

Labels (1)
0 Kudos
Reply
2 Replies

2,248 Views
Pat
Contributor III
0 Kudos
Reply

2,248 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

We offer such complete driver.

You can find it on our web site here:AUTOSAR Software Solutions|NXP

But be aware that it is not free of charge.

Peter

0 Kudos
Reply