breakpoint installation failed: remote communication error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

breakpoint installation failed: remote communication error

Jump to solution
3,011 Views
lixu
Contributor II

    When I use  Design Studio for Power Architecture Version 2.1  for project compilation, it shows "Breakpoints installation failed: remote communication".

   I'm just beginning to learn this and this problem has been bothering me for a long time.

   Please answer me, thanks.

 

0 Kudos
Reply
1 Solution
3,001 Views
Questioner
Contributor II

Same Error had occured for me also, I think you have enabled skip all breakpoints options.

RUN->skip breakpoints.

View solution in original post

4 Replies
3,002 Views
Questioner
Contributor II

Same Error had occured for me also, I think you have enabled skip all breakpoints options.

RUN->skip breakpoints.

2,982 Views
lixu
Contributor II

Thank you. This is exactly the solution I wanted. It's very useful!

0 Kudos
Reply
3,003 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Could you provide more details?

In which phase you are setting breakpoints? Isn't is when the debug session is running?

 

best regards,

Peter

0 Kudos
Reply
2,979 Views
lixu
Contributor II

The problem has been solved. Thank you for your attention!

 

0 Kudos
Reply