XXXX Bus Error - No Opcode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

XXXX Bus Error - No Opcode

7,484 Views
langwu
Contributor I

When I debug TRK-MPC5604B with codewarrior 2.10, I see below issue:

_start XXXX Bus Error - No Opcode

Error: Error in Once status register during instruction execution.

use 'gotil main' command to run until main procedure

Labels (1)
0 Kudos
Reply
1 Reply

4,110 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this might be caused by debugger memory window being opened pointing to illegal/uninitialized memory when the debugger is starting. Also if variables are displayed in Variable window. If this is the case I'd suggest you to close the memory window (or set the address to 0), remove variables from Variable Window  and reset the MCU or download the code again.

BR, Petr