XBAR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

XBAR

2,718 Views
abdelrhman
Contributor III

if HPE (high priority elevation) is enabled, in which cases the master may raise its priority ?? 

0 Kudos
Reply
6 Replies

2,698 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

On this device only FlexRay module is capable to elevate XBAR priority. I am looking for the mechanism.

davidtosenovjan_0-1642606724325.pngdavidtosenovjan_0-1642606724325.png

 

0 Kudos
Reply

2,692 Views
abdelrhman
Contributor III

so, in which scenarios the flexray may send high priority request?

0 Kudos
Reply

2,609 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I just obtained an answer from design

Flexray: The flexray’s high priority signal to the platform is tied high. Thus, if the flexray HPE bit is set, then all flexray transactions are considered high priority.

However I just noticed there is also addendum in RM telling that HPE also works with CPU and DMA

davidtosenovjan_0-1644496179422.pngdavidtosenovjan_0-1644496179422.png

I am apologizing I haven't noticed.

0 Kudos
Reply

2,661 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

This is not clear to us. We have send a question to the design as it seems not to be comprehensively documented. I will return to you as I can.

0 Kudos
Reply

2,706 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Could you specify used device?

0 Kudos
Reply

2,702 Views
abdelrhman
Contributor III

MPC5744p

0 Kudos
Reply