XBAR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

XBAR

2,785件の閲覧回数
abdelrhman
Contributor III

if HPE (high priority elevation) is enabled, in which cases the master may raise its priority ?? 

0 件の賞賛
返信
6 返答(返信)

2,765件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

On this device only FlexRay module is capable to elevate XBAR priority. I am looking for the mechanism.

davidtosenovjan_0-1642606724325.png

 

0 件の賞賛
返信

2,759件の閲覧回数
abdelrhman
Contributor III

so, in which scenarios the flexray may send high priority request?

0 件の賞賛
返信

2,676件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

I just obtained an answer from design

Flexray: The flexray’s high priority signal to the platform is tied high. Thus, if the flexray HPE bit is set, then all flexray transactions are considered high priority.

However I just noticed there is also addendum in RM telling that HPE also works with CPU and DMA

davidtosenovjan_0-1644496179422.png

I am apologizing I haven't noticed.

0 件の賞賛
返信

2,728件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

This is not clear to us. We have send a question to the design as it seems not to be comprehensively documented. I will return to you as I can.

0 件の賞賛
返信

2,773件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Could you specify used device?

0 件の賞賛
返信

2,769件の閲覧回数
abdelrhman
Contributor III

MPC5744p

0 件の賞賛
返信