Why they restore flash controller cache after flash operations?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why they restore flash controller cache after flash operations?

ソリューションへジャンプ
1,701件の閲覧回数
kerem0101
Contributor II

I am using mpc5777c microcontroller. I see these codes in nxp flash code examples. I don't understand why they restore flash controller cache after flash operations. As I understand RestoreFlashControllerCache function enable P0_BFEN and P1_BFEN registers after disabling the these registers. First disable the flash controller cache and after some flash operations, enable the flash controller cache. I don't understand why they enable the cache after these operations.

 

#include "Cpu.h"
#include "flash_c55_driver.h"
volatile int exit_code = 0;
/* User includes (#include below this line is not maintained by Processor Expert) */
/* Lock State */
#define UNLOCK_LOW_BLOCKS 0x00000000U
#define UNLOCK_MID_BLOCKS 0x00000000U
#define UNLOCK_HIGH_BLOCKS 0x00000000U
#define UNLOCK_FIRST256_BLOCKS 0x00000000U
#define UNLOCK_SECOND256_BLOCKS 0x00000000U
/* buffer size */
#define BUFFER_SIZE_BYTE 0x1000U
#define BLOCK_START_ADDRS 0x00000000U
#define BLOCK_END_ADDRS 0x0000FFFFU
#define NUMBER_OF_WORD_BLANK_CHECK 0x90
#define NUMBER_OF_WORD_PGM_VERIFY 0x80
#define NUMBER_OF_WORD_CHECK_SUM 0x120
/* Platform Flash */
#define FLASH_FMC PFLASH_BASE
#define FLASH_PFCR1 0x000000000U
#define FLASH_PFCR2 0x000000004U
#define FLASH_FMC_BFEN_MASK 0x000000001U
uint32_t g_usrCnt = 0U;
uint32_t buffer[BUFFER_SIZE_BYTE / C55_WORD_SIZE];
flash_context_data_t pCtxData;
void UserCallBack(void)
{
/* increase g_usrCnt */
g_usrCnt++;
}
/**************************************************************
* Disable Flash Cache *
***************************************************************/
void DisableFlashControllerCache(uint32_t flashConfigReg,
uint32_t disableVal,
uint32_t *origin_pflash_pfcr)
{
/* Read the values of the register of flash configuration */
*origin_pflash_pfcr = REG_READ32(FLASH_FMC + flashConfigReg);
/* Disable Caches */
REG_BIT_CLEAR32(FLASH_FMC + flashConfigReg, disableVal);
}
/*****************************************************************
* Restore configuration register of FCM *
******************************************************************/
void RestoreFlashControllerCache(uint32_t flashConfigReg,
uint32_t pflash_pfcr)
{
REG_WRITE32(FLASH_FMC + flashConfigReg, pflash_pfcr);
}
/*!
\brief The main function for the project.
\details The startup initialization sequence is the following:
* - startup asm routine
* - main()
*/
int main(void)
{
status_t ret = STATUS_SUCCESS;
uint32_t blkLockState; /* block lock status to be retrieved */
flash_block_select_t blockSelect;
flash_state_t opResult;
uint32_t numOfWordCycle;
uint32_t dest; /* destination address */
uint32_t size; /* size applicable */
uint32_t source; /* source address for program and verify */
uint32_t failedAddress; /* save the failed address in flash */
uint32_t sum; /* check sum result */
uint32_t i; /* Index */
uint32_t pflash_pfcr1, pflash_pfcr2;
/*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/
#ifdef PEX_RTOS_INIT
PEX_RTOS_INIT(); /* Initialization of the selected RTOS. Macro is defined by the RTOS component. */
#endif
/*** End of Processor Expert internal initialization. ***/
/* Invalidate flash controller cache */
DisableFlashControllerCache(FLASH_PFCR1, FLASH_FMC_BFEN_MASK, &pflash_pfcr1);
DisableFlashControllerCache(FLASH_PFCR2, FLASH_FMC_BFEN_MASK, &pflash_pfcr2);
/**************************************************************************/
/* Initialize source buffer */
/**************************************************************************/
for (i = 0; i < (BUFFER_SIZE_BYTE / C55_WORD_SIZE); i++)
{
buffer[i] = 0x0U;
}
/* Flash Initialization */
ret = FLASH_DRV_Init();
DEV_ASSERT(ret == STATUS_SUCCESS);
/**************************************************************************/
/* Lock to protect UTest address space */
/**************************************************************************/
ret = FLASH_DRV_GetLock(C55_BLOCK_UTEST, &blkLockState);
if (!(blkLockState & 0x00000001U))
{
ret = FLASH_DRV_SetLock(C55_BLOCK_UTEST, 0x1U);
if (STATUS_SUCCESS != ret)
{
return ret;
}
}
/**************************************************************************/
/* Unlock all blocks in low address space */
/**************************************************************************/
ret = FLASH_DRV_SetLock(C55_BLOCK_LOW, UNLOCK_LOW_BLOCKS);
if (STATUS_SUCCESS != ret)
{
return ret;
}
/**************************************************************************/
/* Unlock all blocks in mid address space */
/**************************************************************************/
ret = FLASH_DRV_SetLock(C55_BLOCK_MID, UNLOCK_MID_BLOCKS);
if (STATUS_SUCCESS != ret)
{
return ret;
}
/**************************************************************************/
/* Unlock all blocks in high address space */
/**************************************************************************/
ret = FLASH_DRV_SetLock(C55_BLOCK_HIGH, UNLOCK_HIGH_BLOCKS);
if (STATUS_SUCCESS != ret)
{
return ret;
}
/**************************************************************************/
/* Unlock all blocks in 256K blocks */
/**************************************************************************/
ret = FLASH_DRV_SetLock(C55_BLOCK_256K_FIRST, UNLOCK_FIRST256_BLOCKS);
if (STATUS_SUCCESS != ret)
{
return ret;
}
ret = FLASH_DRV_SetLock(C55_BLOCK_256K_SECOND, UNLOCK_SECOND256_BLOCKS);
if (STATUS_SUCCESS != ret)
{
return ret;
}
/**************************************************************************/
/* Call FLASH_DRV_Erase, FLASH_DRV_BlankCheck, FLASH_DRV_Program, */
/* FLASH_DRV_ProgramVerify, FLASH_DRV_CheckSum functions */
/**************************************************************************/
blockSelect.lowBlockSelect = 0x1U;
blockSelect.midBlockSelect = 0x0U;
blockSelect.highBlockSelect = 0x0U;
blockSelect.first256KBlockSelect = 0x0U;
blockSelect.second256KBlockSelect = 0x0U;
g_usrCnt = 0U;
/* Erase block */
ret = FLASH_DRV_Erase(ERS_OPT_MAIN_SPACE, &blockSelect);
if (STATUS_SUCCESS == ret)
{
do
{
/* The user can do any tasks while check status function is still in progress */
UserCallBack();
ret = FLASH_DRV_CheckEraseStatus(&opResult);
}while(ret == STATUS_FLASH_INPROGRESS);
}
if (STATUS_SUCCESS != ret)
{
return ret;
}
dest = BLOCK_START_ADDRS;
size = BLOCK_END_ADDRS + 1 - BLOCK_START_ADDRS;
numOfWordCycle = NUMBER_OF_WORD_BLANK_CHECK;
/* Blank check */
ret = FLASH_DRV_BlankCheck(dest,
size,
numOfWordCycle,
&failedAddress,
NULL_CALLBACK);
if (STATUS_SUCCESS != ret)
{
return ret;
}
/* Program to beginning of block */
dest = BLOCK_START_ADDRS;
size = BUFFER_SIZE_BYTE;
source = (uint32_t)buffer;
g_usrCnt = 0U;
ret = FLASH_DRV_Program(&pCtxData,
dest,
size,
source);
if (STATUS_SUCCESS == ret)
{
do
{
/* The user can do any tasks while check status function is still in progress */
UserCallBack();
ret = FLASH_DRV_CheckProgramStatus(&pCtxData, &opResult);
}while(ret == STATUS_FLASH_INPROGRESS);
}
if (STATUS_SUCCESS != ret)
{
return ret;
}
numOfWordCycle = NUMBER_OF_WORD_PGM_VERIFY;
/* Program verify */
ret = FLASH_DRV_ProgramVerify(dest,
size,
source,
numOfWordCycle,
&failedAddress,
NULL_CALLBACK);
if (STATUS_SUCCESS != ret)
{
return ret;
}
numOfWordCycle = NUMBER_OF_WORD_CHECK_SUM;
/* Check sum */
ret = FLASH_DRV_CheckSum(dest,
size,
numOfWordCycle,
&sum,
NULL_CALLBACK);
if ((STATUS_SUCCESS != ret) && (sum != 0U))
{
return ret;
}
/* Restore flash controller cache */
RestoreFlashControllerCache(FLASH_PFCR1, pflash_pfcr1);
RestoreFlashControllerCache(FLASH_PFCR2, pflash_pfcr2);
/*** Don't write any code pass this line, or it will be deleted during code generation. ***/
/*** RTOS startup code. Macro PEX_RTOS_START is defined by the RTOS component. DON'T MODIFY THIS CODE!!! ***/
#ifdef PEX_RTOS_START
PEX_RTOS_START(); /* Startup of the selected RTOS. Macro is defined by the RTOS component. */
#endif
/*** End of RTOS startup code. ***/
/*** Processor Expert end of main routine. DON'T MODIFY THIS CODE!!! ***/
for(;;) {
if(exit_code != 0) {
break;
}
}
return exit_code;
/*** Processor Expert end of main routine. DON'T WRITE CODE BELOW!!! ***/
} /*** End of main routine. DO NOT MODIFY THIS TEXT!!! ***/
/* END main */

0 件の賞賛
返信
1 解決策
1,671件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @kerem0101 

this is rather relic from older devices where this operation was needed to ensure coherency between flash array and flash line buffers (flash controller cache). If the flash is modified by program or erase function, this operation is supposed to ensure that flash line buffers will be always up to date and you will never read/fetch old data cached before the program/erase operation.

However, this is not necessary on MPC57xx devices. Please take a look at:

https://community.nxp.com/t5/MPC5xxx/MPC5748G-Flash-example-code-question-DisableFlashControllerCach...

Regards,

Lukas

元の投稿で解決策を見る

2 返答(返信)
1,666件の閲覧回数
kerem0101
Contributor II

Thank you!

0 件の賞賛
返信
1,672件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @kerem0101 

this is rather relic from older devices where this operation was needed to ensure coherency between flash array and flash line buffers (flash controller cache). If the flash is modified by program or erase function, this operation is supposed to ensure that flash line buffers will be always up to date and you will never read/fetch old data cached before the program/erase operation.

However, this is not necessary on MPC57xx devices. Please take a look at:

https://community.nxp.com/t5/MPC5xxx/MPC5748G-Flash-example-code-question-DisableFlashControllerCach...

Regards,

Lukas