Just like this,after initializing all the components,i send a"Hello world"message to the terminal by LinFlexD[1],but it display garbled code!
 B46399
		
			B46399
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
I used to face a similar problem in the past; for some reason, when routing the LINFLEXD tx signal to the pin, the logic state of the pin is not correctly driven by the module, instead it remains on a logic 0, so spurious bits may be detected by the terminal interface. A workaround for this issues was to enable the pull up function for the tx pin, so the serial communication bus remains on logic 1 when idle (detecting a 0 actually means the start bit of a character, which is the right behavior).
To enable pull up function, select PinSettings component, go to Functional properties tab, filter the pin name and select the two options as highlighted below:
Please let us know if this fixes the issue!
Regards,
Vlad
 
					
				
		
Hi Vlad,
I did as you told me, but i can't even generate code successfully.
here are the errors:
Regards
 B46399
		
			B46399
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello,
Can you please confirm that you are using SDK 0.8.0? We recently released SDK 0.8.1, the update for Design Studio should be available these days; I recommend updating to the newer version, the pinsettings component was not fully functional in the first release. In the meanwhile, you could try to access directly the appropriate MSCR register in SIUL2 and set the pullup function in the code. Please let me know if this fixes the issue.
Regards,
Vlad
 
					
				
		
Hi Vlad,
I'm sure that my SDK version is 0.8.0.In fact,I already access directly the appropriate MSCR register in SIUL2 and set the pullup function in the code,but it doesn't work for me
This is my pin initialization function.
Regards
 B46399
		
			B46399
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
Can you please share your project? I can't figure out why you get this behavior, I must take a closer look.
One more question: which word length did you configure for UART? 8-bits or 7-bits+parity?
Thanks,
Vlad
 
					
				
		
 
					
				
		
 martin_kovar
		
			martin_kovar
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello,
which do you use?
If you use MPC5748G DEVKIT DEVKIT Evaluation Board for MPC574xG|NXP there is a bug in OpenSDA interface, which causes this issue.
Regards,
Martin
 
					
				
		
Hello Martin,
I use this board,and i known this bug in OpenSDA interface,so i use another LinFlexD_uart which connect to the pin pc[6] and pc[7],but when i transmit data,i still run into this problem!
I found that when i choose display the data in HEX,the 57 became D7,61 became E1,62 became E2,64 became E4,and so on.
When i use the same configuration debugging project without FreeRTOS,i can achieve the correct data.
How can i solve this problem?
I transmit this message to the terminal
The result in FreeRTOS project is
The result in a single LinFlexD_uart project is
Both the project are MPC57xx EAR SDK v0.8.0 Example Project,and i generate the code by PE.
Regards
 
					
				
		
 martin_kovar
		
			martin_kovar
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello,
thanks for your report. It is possible, there is a bug in FreeRTOS module. I will contact SDK development team to investigate this behavior.
Regards,
Martin
 
					
				
		
Hi Martin,
Thanks for your attention.Hope to receive your reply about the solution as soon as possible.
Regards