Using MPC5777C Data cache as SRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using MPC5777C Data cache as SRAM

3,045 Views
Kothe1995
Contributor I

Wanted to use MPC5777C 16kB data cache as SRAM. Need to understand how to configure data cache as SRAM and also at what address space of MPC5777C data cache is available.

0 Kudos
Reply
5 Replies

3,021 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

A procedure you may find in the section 9 (DCache is configured the same way as unified cache on MPC5500

https://www.nxp.com/docs/en/application-note/AN2865.pdf

Possibly I could offer my example code for MPC5676R which device is using the same core, so Dcache configuration (file Optimizations.c) is compatible:

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-XPC567XRKIT-PinToggleStationery-CW210/ta...

It is needed to create virtual address space according to DCache size out of used ranges for other memories.

Possibly following thread could be useful for you:

https://community.nxp.com/t5/MPC5xxx/Dcache-as-RAM-in-MPC5777C/m-p/1660816/highlight/false#M23737

0 Kudos
Reply

3,012 Views
Kothe1995
Contributor I

I wanted to disable data cache and use the data cache memory as SRAM, that means the SRAM space will increase by 16kb of data cache. I also wanted to verify it by using the data cache address in the way we access SRAM. 

0 Kudos
Reply

2,940 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it can be done Actually on this device is is common practice to put stack to the locked cache. As this device is not equipped with TCM (i.e. DMEM) memory, cache is the fastest local memory.

For instance in this example code you may see it as part of startup (init.s):
https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-PinToggleStationery-GHS714/ta-p...

0 Kudos
Reply

2,886 Views
Kothe1995
Contributor I
init.s is not present in above example code
0 Kudos
Reply

2,844 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I can see it there.

davidtosenovjan_0-1695370696112.png

 

0 Kudos
Reply