Using Ethernet port for alternate functionality

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using Ethernet port for alternate functionality

ソリューションへジャンプ
1,901件の閲覧回数
pavangidaveer
Contributor II

Hello,

 

In mpc5200B, we have configured Ethernet port (bit 12:15) of GPS PORT Configuration Register (MBAR + 0B00h) as 1010 (i,e. Two UARTes, J1850).

While in this configuration, we are not using ETH_8, ETH_15 & ETH_16 pins for its specified functionality i.e, UART5e_CD, UART4_CTS & UART4_CD respectively. Rather, we want to use these pins as GPIO, i.e, we want to read and write from/to these pins as in GPIO configuration without configuring Ethernet port (bit 12:15) of GPS PORT Configuration Register (MBAR + 0B00h) as 0000 (i.e, GPIO).

 

Could you please suggest us the method to achieve that?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,788件の閲覧回数
Pavel
NXP Employee
NXP Employee

If the MPC5200B Ethernet is configured using the GPS PORT Configuration Register (MBAR 0B00h) as 1010, the ETH8 is UART5e_CD, the ETH15 is UART4_CTS and ETH16 is UART4_CD signals. These pins cannot be uses as GPIO for this configuration. See the Figure 2-9 of the MPC5200B User's Manual.

You can use CD (carrier detect) signals as GPIO inputs using Input Port Change Register. See the Table 15-13 of the MPC5200B Reference Manual.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,789件の閲覧回数
Pavel
NXP Employee
NXP Employee

If the MPC5200B Ethernet is configured using the GPS PORT Configuration Register (MBAR 0B00h) as 1010, the ETH8 is UART5e_CD, the ETH15 is UART4_CTS and ETH16 is UART4_CD signals. These pins cannot be uses as GPIO for this configuration. See the Figure 2-9 of the MPC5200B User's Manual.

You can use CD (carrier detect) signals as GPIO inputs using Input Port Change Register. See the Table 15-13 of the MPC5200B Reference Manual.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------