Updating MasterECUKey using KDF

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Updating MasterECUKey using KDF

2,563 Views
ayeshap
Contributor I

Dear All,

I'm working on Hardware Security Module which is SHE compliant. While I'm updating Master ECU Key for first time using KDF, when LOAD_KEY command is issued to derive M4 and M5, I'm getting ERC_KEY_UPDATE_ERROR (0x8).

Even after going through HSMSecurity Firmware Manual and knowing all possibilities of getting (0x8) Error code and taking care of those scenarios, still the  Error persists. 

Can anyone suggest a solution?

Thank you.

Tags (1)
0 Kudos
Reply
3 Replies

2,432 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

First of all, please share with us the HSM FW version you are using.

Is it basic or standard version?

regards,

Peter

0 Kudos
Reply

2,432 Views
ayeshap
Contributor I

Hi danielmartynek,

Thanks for the response. I did not realize that this post is in S32K community space. I'm using MPC5748G micro.

Best Regards,

Ayesha

0 Kudos
Reply

2,432 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi [email protected],

What MCU are you using?

S32K1xx does not have HSM, and this post is in the S32K community space.

BR, Daniel 

0 Kudos
Reply