Updating MasterECUKey using KDF

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Updating MasterECUKey using KDF

2,547件の閲覧回数
ayeshap
Contributor I

Dear All,

I'm working on Hardware Security Module which is SHE compliant. While I'm updating Master ECU Key for first time using KDF, when LOAD_KEY command is issued to derive M4 and M5, I'm getting ERC_KEY_UPDATE_ERROR (0x8).

Even after going through HSMSecurity Firmware Manual and knowing all possibilities of getting (0x8) Error code and taking care of those scenarios, still the  Error persists. 

Can anyone suggest a solution?

Thank you.

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,416件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

First of all, please share with us the HSM FW version you are using.

Is it basic or standard version?

regards,

Peter

0 件の賞賛
返信

2,416件の閲覧回数
ayeshap
Contributor I

Hi danielmartynek,

Thanks for the response. I did not realize that this post is in S32K community space. I'm using MPC5748G micro.

Best Regards,

Ayesha

0 件の賞賛
返信

2,416件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi [email protected],

What MCU are you using?

S32K1xx does not have HSM, and this post is in the S32K community space.

BR, Daniel 

0 件の賞賛
返信