Underlying driver codes for MPC5606E

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Underlying driver codes for MPC5606E

1,759 Views
helenshao
Contributor II

Dear Sir/Madam,

 

I'm now doing a project using MPC5606E for Ethernet communication, but I can't find any underlying driver code for MPC5606E on your website, such as clock, CAN, Ethernet, etc.

It's really difficult for me to develop the driver code by myself and I don't have so much time to develop.

So, could you please share me the underlying driver codes for MPC5606E? If you couldn't share all the underlying driver codes, could you please share me a demo code of Ethernet communication of MPC5606E?

 

Many thanks in advance!

Labels (1)
0 Kudos
Reply
2 Replies

1,569 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

There is MPC5604EKIT development kit:

http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/mpc5xxx-5x...

For that kit reference application may be downloaded:

https://www.nxp.com/webapp/sps/download/license.jsp?colCode=FSL-REFKIT-MPC564E&appType=file1&locatio...

This application requires to have installed

Freescale AUTOSAR OS/MPC560xE v.3.0 RTM

in case reference application needs to be modified

Note that AUTOSAR is paid SW:

http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/16-bit-s12-s12x-mcus...

Otherwise this device is very similar to MPC5604P device, thus lot of software examples should be possible to apply to MPC5604E.

You could browse our community space or submit new case (direct question to technical support) with description of required example code and we will see if we have some or not.

Also I could recommend to see simple cookbook AN2865 what may be good starting point:

http://cache.freescale.com/files/32bit/doc/app_note/AN2865.pdf

0 Kudos
Reply

1,569 Views
helenshao
Contributor II

Dear David,

thanks a lot for your help! I have not bought Freescale AUTOSAR OS/MPC560xE v.3.0 RTM and I don't have so much money to buy because I'm only a student in a university. And the kit reference application is too simple and I can't understand. In addition, MPC5604P doesn't have Ethernet module so I can't apply its software examples on MPC5606E.

I want to realize Ethernet communication between two MPC5606EEVB, so could you please share me a demo code of Ethernet communication on MPC5606E and show me how to realize the Ethernet communication? Please give me some details.

Many thanks in advance!

0 Kudos
Reply